9/1/2018 6:55 PM | |
Posts: 11 Rating: (0) |
Boa Tarde, gostaria de pedir ajuda sobre o IM 365, vou iniciar a configuração e instalação, como é uma primeira vez que fazer ... Pedir para me passar um tutorial de dicas ... Começo com qual configuração? Que numero máximo de posso instalar um rack 0 (central) e rack 1 (expanção)? Desde já agradeço a atenção. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 9/3/2018 11:21:07 AMNew subject after splitting |
|
9/1/2018 8:07 PM | |
Joined: 9/27/2006 Last visit: 6/6/2024 Posts: 12260 Rating: (2670)
|
Translation from th Portuguese text.
Olá Scardua; Os membros do fórum da Siemens vêm de muitos países e a maioria não entende português. Por favor, tente escrever em inglês, nossa língua de intercâmbio internacional escolhida, na sua próxima visita. A maior parte do que você está perguntando já foi explicado nas postagens anteriores deste tópico. Só posso sugerir que você leia o Capítulo 8 deste manual para obter explicações sobre o IM 365 e consulte a captura de tela anexada. S7-300 Module Data : https://support.industry.siemens.com/cs/ww/en/view/8859629 Um detalhe: uma vez que os módulos do IM 365 foram conectados na base e re-empilhamento do S7-300, você pode configurar 8 módulos em cada rack. Eles podem ser módulos de sinal (SM), processadores de comunicação (CP) ou módulos de função (FM) no rack base (rack 0); você só pode ter SMs no rack remoto (Rack1). Hello Scardua; Members on the Siemens forum come from many countries, and most do not understand Portuguese. Please try to write in English, our chosen international exchange language, on your next visit. Most of what you are asking has already been explained in the earlier posts of this thread. I can only suggest you read Chapter 8 in this manual for explanations on the IM 365, and refer to the attached screenshot. S7-300 Module Data : https://support.industry.siemens.com/cs/ww/en/view/8859629 One detail: once the IM 365 modules have been connected on the base and reote racks of the S7-300, you can setup 8 modules on each rack. They can be Signal modules (SM), Communication processors (CP) or Function modules (FM) on he base rack (Rack 0); you can only have SMs in the remote rack (Rack1). Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
9/3/2018 12:29 AM | |
Posts: 11 Rating: (0) |
Good night, thank you very much for your attention. I have been reading the manual and what worried me was consumption, the IM 365 releases by 800ma correct rack? Backplane bus would be the consumption of each card in this 800ma per rack? According to manual mount 8 rack cards 0 (AI8x12bit) with consumption in the backplane of 50ma each, totaling 400ma. And it would mount in rack 1 (extension) 3 cards (DI16xDO16x24v) with consumption of 80ma each, totalizing 240ma and 3 cards (AO8x12bit) with consumption 100ma each, totaling 300ma. In rack 0 would be consumption of 400ma, and rack 1 (extension) consumption 540ma. It would be 400 + 240 + 300 = total 940ma Now tell me, is the information I've written correct? or I'm missing something. I thank the attention |
Last edited by: Jen_Moderator at: 9/3/2018 11:23:45 AMEdited text for better reading. |
|
9/3/2018 7:54 PM | |
Posts: 11 Rating: (0) |
Thank you, for all information, maybe may translator has switched to Portuguese, sorry. All information were very useful. |
Follow us on