3/28/2022 9:20 AM | |
Joined: 2/17/2020 Last visit: 7/16/2024 Posts: 1022 Rating: (180) |
Hi, How have you configured the PG/PC interface? Are you trying to communicate a simulated S7-1500 and a WinCC Unified Runtime? If so, please check out this FAQ. Is the PLC protected? Make sure it allows 'HMI Access'. Also, check that the PLC Tags, in the PLC Tags table, are configured as 'Accessible from HMI/OPC'. |
A rating will be well appreciated. |
|
3/28/2022 10:48 AM | |
Joined: 2/24/2020 Last visit: 7/8/2024 Posts: 10 Rating: (0) |
Yes, all have been configured. The version of TIA Portal is V17. Any suggestions? |
3/28/2022 11:14 AM | |
Joined: 2/24/2020 Last visit: 7/8/2024 Posts: 10 Rating: (0) |
Here it is |
3/28/2022 12:05 PM | |
Joined: 2/24/2020 Last visit: 7/8/2024 Posts: 10 Rating: (0) |
Okay, thanks a lot. |
This contribution was helpful to1 thankful Users |
Follow us on