2/14/2017 9:46 AM | |
Joined: 10/17/2011 Last visit: 7/19/2022 Posts: 148 Rating: (3) |
hello, I have laptop with windows10 operating system. In that, I have installed virtual machine with Windows7 professional 64bit and installed STEP7 V5.5 SP4 on virtual machine. Simatic manager is working fine but I am not able to open help file. If I tried to open it, it shows" Failed to launch help S7KAFAPX" I downloaded windows help file Windows6.1-KB917607-x64 Windows6.1-KB917607-x86 I started virtual machine and tried to run above file. but none of the above files can be installed. If I try to install it, it gives error "Installer encountered an error: 0x80070422 The service can not be started,either because it is disabled or because it has no enabled devices associated with it." Please help me to resolve this. Thank you, Damayanti ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 2/14/2017 2:24:08 PMNew subject after splitting |
|
2/15/2017 6:15 AM | |
Joined: 11/5/2012 Last visit: 8/10/2024 Posts: 487 Rating: (63) |
Hello Damayanti. I think this might help you: Someone else had a similar problem. regrads |
Follow us on