1/15/2018 10:22 AM | |
Joined: 4/28/2015 Last visit: 5/15/2024 Posts: 3345 Rating: (377)
|
Hi, this is possible using node-red. You can use the S7 node to get data from your ET200S CPU. Here is an application example using a S7-1500. There is a node for sending push notifications to smartphones as well: https://flows.nodered.org/node/node-red-contrib-push. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
1/19/2018 9:37 AM | |
Joined: 4/13/2016 Last visit: 1/15/2024 Posts: 3 Rating: (0) |
HI Bergmanu Thanks for your reply we will look further into this. Right now we are also discussing to develop an app to android which could either talk directly with the PLC. And then have some code in the PLC to send directly to this app. We already have an App that Works som of the way. But i would rather have the IOT in between so that it would be minimal that we need to do in the PLC. So now the IOT2040 is ordered and i will get to play with it.. :-) |
This contribution was helpful to1 thankful Users |
Follow us on