6/18/2009 5:50 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (308) |
Hello, Did you have a look here? http://support.automation.siemens.com/WW/view/en/31622970 Notify_8p is listed. |
Best regards |
|
6/19/2009 9:17 PM | |
Joined: 3/18/2009 Last visit: 5/6/2024 Posts: 306 Rating: (94) |
Hello Tuff Gong,
Let me know, if this is what you were looking for. regards. Edit
WinCC has only one messaging system. So in the end even the operator log will be in the alarm log. Your comment about it not appearing as an alarm will need (as in PCS7) a clever segregation of messages using message classes (and other properties) and their subsequent display in alarm control object by proper filtering. hope it helps. Edit: Ok, the property "Operator Input Message" also exists for buttons as pointed out by Tuff Gong in the posts below. Thanks Tuff. |
Last edited by: daga at: 6/24/2009 11:55 AMLast edited by: daga at: 6/19/2009 9:25 PM |
|
6/20/2009 11:50 AM | |||
Joined: 4/5/2006 Last visit: 6/25/2024 Posts: 917 Rating: (63) |
Hi Tuff, in add to waht dagasaid, have a look to this FAQ
Hope can help you Regards |
||
6/24/2009 10:32 AM | |
Posts: 41 Rating: (1) |
Hi, What I was looking for is the "Operator Input" property. It does exist on buttons from V6.2. Thank you for your help. |
6/24/2009 11:11 AM | |
Posts: 41 Rating: (1) |
Hi Daga, I use a direct connection on my button, then it's available. AttachmentOperator Input.pdf (194 Downloads) |
This contribution was helpful to1 thankful Users |
6/24/2009 11:44 AM | |
Joined: 3/18/2009 Last visit: 5/6/2024 Posts: 306 Rating: (94) |
Thanks a ton. |
Follow us on