5/24/2019 5:38 PM | |
Posts: 24 Rating: (3) |
Hello again, I have another question, I thought about creating a new post, but since someone told that you two are among the best experts in the forum, I chose to post it here as a reply. well, it is a similar problem, I tried to install "node-red-contrib-s7" but I couldn't. I had this error message. root@iot2000:~# cd /usr/lib/node_modules root@iot2000:/usr/lib/node_modules# npm install node-red-contrib-s7 npm ERR! Linux 4.4.105-cip15 npm ERR! argv "/usr/bin/node" "/usr/bin/npm" "install" "node-red-contrib-s7" npm ERR! node v6.12.3 npm ERR! npm v3.10.10 npm ERR! code CERT_NOT_YET_VALID npm ERR! certificate is not yet valid npm ERR! npm ERR! If you need help, you may report this error at: npm ERR! <https://github.com/npm/npm/issues> npm ERR! Please include the following file with any support request: npm ERR! /usr/lib/node_modules/npm-debug.log I also runned "npm install -g node-red-contrib-s7 --build-from-source" but the result is the same. Best regards, ------------------------------------------------------------------------------------------ Attachmentnpm-debug.txt (188 Downloads) |
Last edited by: tipstn at: 05/24/2019 18:33:54Last edited by: Jen_Moderator at: 05/27/2019 10:22:34New subject after splitting Last edited by: Jen_Moderator at: 05/27/2019 10:44:26Optimized headline. |
|
5/29/2019 7:11 PM | |
Posts: 24 Rating: (3) |
Thank you, It worked. |
Follow us on