11/2/2023 6:05 AM | |
Joined: 3/14/2008 Last visit: 10/15/2024 Posts: 2111 Rating: (942)
|
Hi, Thr PH works a bit different. The PH is made up levels top to bottom. If you have set this option, you will get three hierarchy folders under each other. With the arrow button, you can go down those levels. Your print screen shows you have three unit folders. 1. Process Cell 2. Unit 3. Function You can get a total of 8 hierarchy levels (can be configured in the Plant Hierarchy settings. See attached screen. You can also choose which PH folder is your start position. If you look at your print screen, your PH starts at the unit level. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on