Industry Online Support
Technical Forum
9/13/2012 2:39 PM | |
Posts: 378 Rating:
|
Hello russ1669 , In order to make bidirectional communication, you need to setup a single device as a Server and Client. On you logosoft goto Tools>Ethernet Connections and right click Ethernet Connections>Add Connection then setup a proper IP adresses. For your Last Question: You can not make a connection not connected to "Output". Output on this context means DI/DO/AI/AO/Digital Flag/Analog Flag/... but if you need to store values to be read and write via network you can use Parameter mapping. I have attached here a sample Server-Client program for two networked LOGO's (I have downloaded from this forum and I can't remember the thread) Regards, AttachmentBasic Bi-Directional Network.zip (640 Downloads) |
Last edited by: desmul24 at: 9/13/2012 2:42 PM |
|
9/13/2012 2:59 PM | |
Posts: 5 Rating:
|
Thankyou Desmul. That network example has given me some ideas. Russ |
Follow us on