4/3/2013 5:44 PM | |
Joined: 12/19/2011 Last visit: 6/2/2022 Posts: 36 Rating: (0) |
Hi! Again turn to you for help. I have two axes of the machine driven by one motor.On each axis encoder her. The motor encoder is connected to the drive and sensor axes to a switching hubDMC20. I first configure the system to work without sensors axes (for position feedback sensor is used engine). Everything is working fine. Now I can not connect the sensor axes for position feedback. Please help me if you can! Attachment333.pdf (87 Downloads) |
Last edited by: spec-cnc at: 4/5/2013 7:47 AM |
|
4/5/2013 7:48 AM | |
Joined: 12/19/2011 Last visit: 6/2/2022 Posts: 36 Rating: (0) |
Please help me if you can!
Attachment444.pdf (91 Downloads) |
Last edited by: spec-cnc at: 4/5/2013 7:51 AM |
|
4/5/2013 8:47 AM | |
Posts: 391 Rating: (50)
|
The function you look for is in the "Manual Special Functions" under "setpoint exchange" explains |
Follow us on