6/7/2010 9:34 AM | |
Joined: 4/29/2010 Last visit: 8/12/2024 Posts: 1557 Rating:
|
It isn`t possible to change the device type of a OP17 because in ProTool it is just possible to project one OP17. The message is caused by the projected connection wich isn`t supportet by the OP17DP. For example if you project a Profibus connection you can`t download this project at a OP17PP because this device doesn`t support a Profibus connection. You can find the manual of the OP17 at this FAQ, there you can also see wich connection types are supported by the different types (PP,DP,DP-12): http://support.automation.siemens.com/WW/view/en/1145112 |
6/16/2010 8:14 AM | |
Posts: 4 Rating:
|
Wizard. |
6/16/2010 8:17 AM | |
Posts: 4 Rating:
|
Thank you Sandman, i have already download the manual i will chek that information |
Follow us on