4/5/2019 8:00 PM | |
Posts: 6 Rating: (0) |
Hello you all, Is possible to use OPC UA to connect a S7-1214C with a PC? |
4/5/2019 9:33 PM | |
Posts: 6 Rating: (0) |
Thanks, but I must know with a CPU 1214C. With a 300 or S71500 I'm sure is possible. |
4/5/2019 9:51 PM | |
Joined: 9/8/2011 Last visit: 8/7/2024 Posts: 537 Rating: (86) |
I'm sorry. Download Kep at : https://www.kepware.com/en-us/products/kepserverex/ Run it on your PC. Set up a connection. Add some tags. Change them on the PLC and see if they change on the PC. I'm sure you will find it works. It installs a client program, you can test with. If its only a few tags you just have the server boot up with those tags available. If its a bunch of array's you may want to create the connections and tags with you PC programmatically. Good Luck. |
A smart person learns from their mistakes |
|
4/5/2019 10:20 PM | |
Posts: 6 Rating: (0) |
OK, Thank you, I'll try this program. Seems really good. I also read something about the s7-200 PC access, what do you think? |
Follow us on