4/8/2022 8:41 AM | |
Joined: 3/11/2019 Last visit: 11/7/2024 Posts: 1653 Rating: (303) |
Dear dang trinh, I am not 100% sure about this error, but you can find something with google. Please also check if the tags "UAMethod_InParameters" and "UAMethod_OutParameters" was configured correctly. As far as i know this tags need this names exactly. But as there are no other answers till this point, maybe a service request would be the best. Maybe this can help in any way, too. OPC_UA_ServerMethodPre: Preparing the server method call OPC_UA_ServerMethodPost: Post preparation of the server method call Example program for providing a method for OPC UA clients regards sancruz |
Feedback appreciated, please rate |
|
This contribution was helpful to1 thankful Users |
4/11/2022 5:24 PM | |
Joined: 9/21/2006 Last visit: 5/25/2023 Posts: 247 Rating: (65) |
For Q2, the diagnostic buffer == System Alarms, so can be read using the Get_Alarm instruction. See Reading out Alarms with the "Get_Alarm" instruction in S7-1500 CPU for details. |
This contribution was helpful to1 thankful Users |
4/12/2022 10:23 AM | |
Joined: 8/3/2009 Last visit: 11/7/2024 Posts: 14112 Rating: (1767) |
Hello dang trinh Here is also a basic FAQ to this topic, perhaps it helps to check first the example: https://support.industry.siemens.com/cs/de/en/view/109756885 Bye Murof |
Last edited by: Murof at: 04/12/2022 10:23:23If this Information really helps, you could use the Rate function |
|
4/12/2022 11:22 AM | |
Joined: 8/3/2009 Last visit: 11/7/2024 Posts: 14112 Rating: (1767) |
Hello dang trinh Here is also a basic FAQ to this topic, perhaps it helps to check first the example: https://support.industry.siemens.com/cs/de/en/view/109756885 Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on