8/18/2022 11:53 AM | |
Joined: 12/24/2016 Last visit: 6/28/2024 Posts: 9 Rating: (0) |
Hi guys, I need some help. I'm using an IOT2040 gateway running Node-Red locally. I'm trying to configure the OPC UA Server node on it, but all attempts end in failure. I used the OPC UA Client node normally and connected the IOT2040 to several different OPC UA Servers, but I can't do the opposite. When I configure my OPC UA Server node and try to get it running I get the following error: Error: get-installed-path: module not found "node-opcua-server" in path /home/root/.node-red/node_modules/node -red-contrib-opcua/node-opcua-server I use the image IOT2040_Example_Image_V3.1.1.zip (454.8 MB) that was downloaded in Entry ID: 109741799. Could you help me to solve this problem please? Attached I will be putting the images of my configuration and the information of the IOT2040.
AttachmentMy Configuration.zip (670 Downloads) |
8/19/2022 9:46 AM | |
Joined: 4/28/2015 Last visit: 6/3/2024 Posts: 3345 Rating: (378)
|
Hi, I tried different things, but did not find a solution.. The required node-opcua-server is located in the path /home/root/.node-red/node_modules/node -red-contrib-opcua/node_modules/node-opcua-server. What I tried:
What I know from the past is that we do not recommend using the OPC UA Server of this node. Details see here. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
11/15/2022 1:18 PM | |
Joined: 8/31/2022 Last visit: 9/8/2023 Posts: 7 Rating: (0) |
Did anyone get an OPC UA Server working with Node-Red? Hello bergmanu, If I were to set up the OPC UA Server, using the guide in your link would it work with node red?
|
Follow us on