2/16/2012 8:34 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating:
|
Hello, Open Pro Tool 1.x configuration with current software Are you sure that file is OP25 project? Because this extension is a Prosave backup file and you can't to open in order to edit it. Only is possible to do a restore on the same type of panel. Best regards, Hristo Mihalev |
2/16/2012 2:50 PM | |
Posts: 3037 Rating:
|
Hello, You can not do a backup of OP25 with Prosave. This is not possible. You must project this function with ProTool. You can see this inthe following manual chapter 13.2 Operator Panel OP25, OP35, OP45 Tweety |
2/16/2012 4:20 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating:
|
Are you sure that psr file regards Op25? Anyway, if you wantsend me that file in order to try it. Or Support Requestlike an options is valid too. Best regards, Hristo Mihalev |
2/16/2012 4:51 PM | |
Posts: 4 Rating:
|
Thanks for your help.... Really I don´t know the origin of the file. I don´t generate it. I attached it to the message, if you want to check it. But, is there any way to make a bakup-restore of OP-25 without original archives? AttachmentOP-25-mercerizadora.zip (370 Downloads) |
Follow us on