4/24/2016 12:09 PM | |
Posts: 94 Rating: (2) |
dear all how to order optical fiber cable and how to fix the optical fiber cable terminal |
4/24/2016 12:14 PM | |
Joined: 3/17/2013 Last visit: 12/25/2023 Posts: 480 Rating: (43) |
Hi In which reference you are asking VFD, PLC etc.!! for example Prefabricated FOC also exists with Siemens Sinamics VFDs. Splicing FOC is explained in so many links, for example http://www.thefoa.org/tech/ref/OSP/term.html Cheers |
4/24/2016 12:28 PM | |
Posts: 94 Rating: (2) |
for vfd |
4/24/2016 1:07 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Please provide complete MLFB number of drive. |
4/24/2016 1:49 PM | |||||||||||||||||
Joined: 9/7/2007 Last visit: 8/30/2023 Posts: 550 Rating: (61) |
Hi alaa There are many types of fiber optic cables and connectors each device has its own type of connector refer to this link and the table below to get more info:
The following fiber optic cables are available for Industrial Ethernet:
The following fiber optic cables are available for PROFIBUS:
|
||||||||||||||||
Best Regards |
|||||||||||||||||
This contribution was helpful to1 thankful Users |
4/25/2016 11:47 AM | |
Joined: 3/1/2013 Last visit: 4/8/2024 Posts: 4 Rating: (0) |
Is the cable used for connecting Simolink SLB boards ? |
4/26/2016 1:14 PM | |
Joined: 9/7/2007 Last visit: 8/30/2023 Posts: 550 Rating: (61) |
Hi Rakky; you can use any FO cable with Simolink SLB as mentioned in the manual:
But you MUST use its own input and its own output connections refer to the attached manual page 4-1 and 4-2
AttachmentSLB.pdf (270 Downloads) |
Best Regards |
|
4/27/2016 6:11 AM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (306) |
Hello This is a useful FAQ regarding FO Cables and Connectors: Which connector do you use to connect fiber-optic cables to the optical interface of network components and terminals? Cheers Navnag |
There is no such thing as the last bug in a program |
|
4/27/2016 9:28 AM | |
Joined: 9/7/2007 Last visit: 8/30/2023 Posts: 550 Rating: (61) |
I have already mentioned this link in my first reply
|
Best Regards |
|
Follow us on