5/2/2008 12:27 AM | |
Posts: 3609 Rating: (29) |
Importing a Techncial Question of an User
|
5/2/2008 6:00 AM | |
Posts: 1064 Rating: (72) |
The p area is the process image of your i/o what error aree you getting? |
5/2/2008 6:04 AM | |
Joined: 9/27/2006 Last visit: 10/8/2024 Posts: 12285 Rating: (2685) |
Hello jitu; P and Q areas were addressing pages used in S5 PLCs to extend the addressing range of those CPUs. At that time, memory was expensive and bulky, and it was necessary to use programming tricks to extend their availability.Maybe you remember that DOS did the same to overcome the 64K limit on computer RAM. In S7 CPUs, there is no longer use for P and Q areas, so the terms are not used anymore. Is this an S5 to S7 conversion problem? In this case maybe the following FAQ has a solution for you: http://support.automation.siemens.com/WW/view/en/1995028 If the source of the message is not from a S5 to S7 conversion problem, could you please give more details? Like the code of the block that is being pointed oput by the compiler? Hope this helps, Daniel Chartier |
5/14/2008 2:50 PM | |
Posts: 24 Rating: (0) |
Dear Sir, The error is communication.I am attaching info.Please suggest . regards, Attachment314C 2DP.pdf (331 Downloads) |
5/14/2008 2:52 PM | |
Posts: 24 Rating: (0) |
Dear Sir, Second attachment is attached, thanks, AttachmentBACKUP_AS_ON_17_3_08_SIMATIC 30.pdf (301 Downloads) |
Follow us on