10/14/2019 2:14 PM | |
Joined: 3/20/2015 Last visit: 7/9/2024 Posts: 59 Rating:
|
Hello, I managed to communicate successfully with PAC3200 through PROFIBUS, but now I would like to communicate with PAC3200 through PROFINET network. I found out that there is a different GSD file which has to be installed in order to communicate through PROFINET (although I'm not sure if is a difference between the GSD for PROFIBUS and PROFINET). Here is the link where I'm supposed to download the GSD from. But I'm redirected to a link where I'm told that: "You have no authorization for the download of export restricted software. For this authorization you have to register once, the authorization is a prerequisite for export-restricted downloads. Click "Continue to registration" to start the registration process.". When I click "Continue to registration", nothing happens. Does anyone have the GSD file or a link where I can download from? Many thanks in advance! |
10/14/2019 2:43 PM | |
Joined: 2/24/2015 Last visit: 1/25/2023 Posts: 306 Rating:
|
|
10/14/2019 3:01 PM | |
Joined: 3/20/2015 Last visit: 7/9/2024 Posts: 59 Rating:
|
Thanks for replying, Konstantin_D! I will try to register following the steps from the link you provided. I am using SIMATIC Manager, not TIA Portal. |
10/15/2019 8:57 AM | |
Joined: 3/20/2015 Last visit: 7/9/2024 Posts: 59 Rating:
|
Thanks a lot for the GSD you sent me yesterday. I installed it but I can't find it in HW catalog. In HW catalog I can find only the GSD used to communicate through PROFIBUS (7KM9 300-0AB01-0AA0). The GSD you gave me (7KM93-0AE01-0AA0) can't be found in HW catalog after its installation. What am I missing? Thanks in advance! |
10/15/2019 9:06 AM | |
Joined: 2/24/2015 Last visit: 1/25/2023 Posts: 306 Rating:
|
I checked on a clean installation - I got it in the HW Catalog. |
Follow us on