2/2/2016 7:40 AM | |
Joined: 3/14/2008 Last visit: 7/12/2024 Posts: 2076 Rating: (930) |
Hello m.anghel, In order to use the functionality: failsafe, you can order the optional package: "S7 F Systems". If you installed this, you have TuV certified CFC blocks available at your disposal. See this link for more information: http://w3.siemens.com/mcms/simatic-controller-software/en/programming-options/s7-f-fh-systems/s7-f-systems/pages/default.aspx And you can download the manual from here (sorry, file size is too large so I can't upload it): I hope this is what your looking for! |
Last edited by: Oreca at: 2/2/2016 7:46:33 AMIf I could help you, you can use the RATE button. Thank you. |
|
2/3/2016 10:28 AM | |
Joined: 3/14/2008 Last visit: 7/12/2024 Posts: 2076 Rating: (930) |
Well, F_Source_add is a unique profisafe address that is assigned automatically and differs from 1 to 65534.. The error can mean a few things: - Profibus connection error - F-Monitoring time in hardware config is set too low - Invalid parameters in hardware config Can you tell me what is in the diagnostic buffer of the F I/O? Have you tried powering the F I/O off and on again?
|
If I could help you, you can use the RATE button. Thank you. |
|
2/3/2016 12:26 PM | |
Joined: 3/14/2008 Last visit: 7/12/2024 Posts: 2076 Rating: (930) |
Did you recompile the S7 program and downloaded to CPU after changing the timeout? Otherwise, I have to check what options more you have.... |
If I could help you, you can use the RATE button. Thank you. |
|
3/7/2016 12:35 PM | |
Joined: 3/24/2010 Last visit: 5/28/2024 Posts: 6 Rating: (0) |
Hi, I have the same problem here did you already find a solution? |
Follow us on