3/4/2008 12:16 AM | |
Posts: 2661 Rating: (279) |
You can safely ignore the warning. It has no impact on the functioning of the program. |
This contribution was helpful to1 thankful Users |
3/4/2008 11:27 AM | |
Posts: 6 Rating: (1) |
Hi Mario. Thanks for the help. I will try to redistribute myruntime groups a bit better. Best Regards Migcooper. "Obrigado Mario" ----------IPB---------- :) |
3/5/2008 7:44 PM | |
Posts: 2661 Rating: (279) |
The warning limit (64K) is the size limit for the (compiled) FC set by the SCL compiler. But I wish this was pointed out more clearly in the help files and the warning logs. In earlier versions (V6.0 and below) when a RTG was not created automatically for every CFC insert, this size limit used to be a major problem. One realized this only after a failed compile and had to rearrange runtime groups/blocks. This warning limit should not be the basis for rearranging runtime groups. In other words, it is possible to “overload” the system withoutever reachingthis limit. AttachmentDokument1.pdf (502 Downloads) |
This contribution was helpful to1 thankful Users |
3/7/2008 8:22 AM | |
Posts: 198 Rating: (17) |
p.s . in a cfc > options > custumize > compile/download > installed blocks per runtime or ob group options... you can adjust that number |
Follow us on