9/1/2018 1:50 PM | |
Joined: 9/9/2015 Last visit: 8/27/2024 Posts: 727 Rating:
|
Hi, Just to understand further, 1. I am not that clear on the system architecture. How many OS Servers do you have? How many clients do you have? Is each zone having its OS servers individually? If yes, it means the OS Server and AS connection has not been established. 2. If both of the zones are using the same OS Servers, can you take a screenshot on the tag management industrial ethernet? 3. Have you compile the OS servers and download with the latest tags? Regards, Jaz |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
9/6/2018 3:57 AM | |
Joined: 9/9/2015 Last visit: 8/27/2024 Posts: 727 Rating:
|
Sorry for late reply, kinda busy recently. Okay, different zone, each zone control by one AS. And the CIP portion is not having a communication with OS. From what i see in Tag management, it is confirmed that the tag is in tag management of the OS servers. Can you press the AS connection which consists of the CIP portion to take a look at the tags? Then make sure the tags are configured correctly in the graphics ? I believe the tags in the graphics are wrong. Thank you. Hope it helps. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on