Industry Online Support
Technical Forum
10/26/2010 3:54 PM | |
Posts: 18 Rating: (0) |
i dont know what should i do next when this icon does show..pls help me with this problem |
10/26/2010 6:00 PM | |
Joined: 9/27/2006 Last visit: 7/14/2024 Posts: 12268 Rating: (2675) |
Hello th0ny; This icon, allong with others, appears during connection of PDM with the PA slaves and is part of the PDM Lifelist diagnostics. Baiscally, it means that it has detected an unusual state inthe particular slave and that it should be looked after, serviced or repaired. If this is a new module,the message could be related to deficient parametrizationthrough PDM; or there might be something wrong in the installation procedures. There is not much more information in the PDM manual, as it relates to the particular slave it is pointing to. So open the slave`s manual, check installation, parametrizationand maintenance recommendations from the manufacturer. Here is a link to the PDM manual, see the information availablethere : PDM V6.0 The Process Device Manager Hope this helps, Daniel Chartier |
Last edited by: O_Moderator at: 10/27/2010 8:49 AMlink edited |
|
Follow us on