3/20/2018 6:37 AM | |
Joined: 3/14/2008 Last visit: 11/14/2024 Posts: 2130 Rating: (953)
|
Hi, Welcome to the Siemens Support Forum! I hope you can find your way around, if not let us know! The picture sizes can be set in the OS project editor in WinCC Explorer of the OS (Server of client). You can set how many screens you want (up to 4) and in which order (square, horizontal). You can choose from a template like SIMATIC Standard 1920*1080 or 1024*768. What happens is that all pictures are resized to fit in those limits you have chosen. Remember that when choosing 1920*1080, you have a height of 1080, but since the process picture consists also of the Overview (Area buttons/PCS7 logo/Clock etc) and Buttons (Buttons for operation of WinCC), the remaining size for your process screen is less. For a height of 1080, the process screen height (where you put your block icons and visualization of the process) is 847. It is possible to create a new template with dimensions you can assign yourself, but that takes some effort. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on