5/26/2023 8:53 AM | |
Joined: 2/24/2020 Last visit: 5/17/2024 Posts: 1 Rating: (0) |
Hi I have a question We are controlling a gas burner with this PID_3step, we have a problem because the transition time of going from 0-100% is diffrent from going from 100-0%. This cause a problem in the regulation. Sometimes we are reaching the Up limit in the controller but the burner is not 100%. Is the a we you can solve this in the PID_3Step or should we use a diffrent PID that doesn´t care about the transition time. In our case it isn´t a fysical actuator in the burner, it is only a value from 0-100%. We need a PID that use a signal for up and down like this PID_3step does. Best regards Markus ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/26/2023 10:52:08New subject after splitting |
|
Follow us on