7/10/2017 5:45 AM | |
Joined: 6/21/2013 Last visit: 7/27/2022 Posts: 13 Rating:
|
Dear! i have 5 PLC S7-300: 315-2AH14-0AB0 and 5 CP: 343-1EX30-0XE0. They have comminucation to 1 switch, together. now, i want to transfer data between them. when i configuration then only 2 PLC OK. I hope you can help me how to i can transfer data all. I use type ISO-on -TCP and block FC5 and FC6 to send and received data. You can give me your email. I can send my project to you check for me. Thanks! Best regards! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 7/10/2017 10:38:07 AMNew subject after splitting |
|
7/10/2017 8:01 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
hi, have a look in this manual, what kind of communication you can use between two S7-CPUs. CPU-CPU Communication with SIMATIC Controllers you can also use the search-bar in the upper right to find a application sample that fits, like this: How do you program the communication blocks FC5 and FC6? hope this helps, regards, |
FCK WAR! |
|
Follow us on