1/10/2014 12:31 PM | |
Joined: 4/24/2006 Last visit: 7/11/2024 Posts: 8711 Rating: (1165) |
Hello @Nick, I try it, but I can choose different interfaces. The difference with your software version is, that I use Step 7 v5.5 + SP3 Service Pack 3 for STEP 7 V5.5 and STEP 7 Professional 2010 Best regards, Wizard |
1/10/2014 12:46 PM | |
Joined: 11/17/2010 Last visit: 11/25/2020 Posts: 81 Rating: (2) |
Hi Wizard, Thanks for your Reply. SP3 is not working on my (new HP)laptop :-( I discussed and triedsolvingit weeks with Siemens. They could not help me beacause there was a dutch version of Windows 7 installed. Strange problems occur with archiving/retreiving and HW-Catalogus in the HW editor etc. It even lead to a blue screen during istallation and made the computer crash. The PLC SIM always worked fine till today. Thanks in advance! |
1/10/2014 1:06 PM | |
Joined: 4/24/2006 Last visit: 7/11/2024 Posts: 8711 Rating: (1165) |
Hello @Nick, hmm, is the Windows pre-installed on Laptop? Because there are known problems with HP notebooks and Siemens software. See also this link: What should you watch out for when installing WinCC flexible 2008 SP3 or WinCC V11 SP2 on an HP notebook? Best regards, Wizard |
5/13/2014 12:30 PM | |
Joined: 3/19/2010 Last visit: 4/17/2024 Posts: 438 Rating: (12) |
Hello I just want to inform audience that I have exactly the same problem. My PLCSIM doesn't work with TCP/IP connection selected. I have read the posts https://www.automation.siemens.com/tf/WW/en/Posts/96737 I have deleted xml file for plcsim.tcp.1 also. Now, I cannot choose TCP/IP connection from PLCSIM. Other connections (MPI, Profibus) work OK. Any new ideas? I have Windows 7 Pro, Step 7 v5.5 upd 2, PLCSIM 5.4... |
5/13/2014 12:59 PM | |
Joined: 1/28/2009 Last visit: 7/11/2024 Posts: 6842 Rating: (1362)
|
Hello, Similar question discussed HERE plus the original support request (in German) suggets , delete those 5 files and restrat.Then check the result. If it is not working try to install them again via Options--> Set PG/PC interface-->Interfaces(Add/Remove). If still no success, contact HERE for more help! Best regards, Hamid Hosseini |
5/13/2014 3:49 PM | |
Joined: 3/19/2010 Last visit: 4/17/2024 Posts: 438 Rating: (12) |
I have installed SP3 for Step7, and reinstalled PLCSIM. Now, it works fine. |
This contribution was helpful to2 thankful Users |
1/8/2015 7:06 AM | |
Joined: 1/10/2011 Last visit: 1/11/2023 Posts: 10 Rating: (0) |
Hi Nick, I have got same problem as you with PLCSIM. Have you got any solution?
|
Follow us on