1/10/2011 10:32 AM | |
Posts: 3 Rating: (0) |
Hello, I am following PCS 7 - Getting Started - Part 1 (09/2007) and have a problem with connection over ethernet between PLCSIM and Station Configurator (WinCC part). I am using only my laptop (want to run WinCC and PLCSIM at the same time) When I download configuration of PC station to Station Configurator all positions (IE General, WinCC Application run - have green icon), but when I open PLCSIM position 1 (IE General) goes to stop mode! When PLCSIM is running and I select: When I select PC station -> PLC -> Configure... and configure button I get warning on first position (IE General) "There is a difference between the MAC address or the IP address of the configured and the existing component. The address of the existing component will be retained" My configuration is the same than in Getting Started, on PC station I am using the same MAC address then network card of my laptop, on the PLC side (CP 443-1) other MAC address. Under NetPro I created S7_connection. look at the attachement (pdf with pic's) am I doing something wrong ? please help I am using PSC7 version V5.4 + SP3 Attachmentconnection_problem.pdf (294 Downloads) |
Follow us on