7/24/2018 8:36 AM | |
Joined: 7/22/2015 Last visit: 11/13/2024 Posts: 23 Rating: (5) |
Installed software attached. |
7/24/2018 8:53 AM | |
Posts: 2826 Rating: (686) |
Hello. You have already the newest updates installed, even for Automation License Manager. Which version Windows (with build number) do you have? Do you have the security patch loaded? - If you have that too and it still is giving problems, please register a formal Support Request. There is a button with same name on this page. Good luck. |
7/24/2018 9:00 AM | |
Joined: 7/22/2015 Last visit: 11/13/2024 Posts: 23 Rating: (5) |
Edit : Tried the patch, there is still the same issue. Here is more information about the OS : |
Last edited by: Ronanf at: 7/24/2018 9:10:46 AM |
|
7/24/2018 9:01 AM | |
Joined: 12/18/2014 Last visit: 11/14/2024 Posts: 34214 Rating: (4261) |
Which licenses shows the license manager? Please make a screenshot |
7/24/2018 9:22 AM | |
Joined: 7/22/2015 Last visit: 11/13/2024 Posts: 23 Rating: (5) |
Formal request done. Let's see. |
7/25/2018 7:07 PM | |
Joined: 7/22/2015 Last visit: 11/13/2024 Posts: 23 Rating: (5) |
Support is not helping that much. I tried a fully fresh install on TIA V15 with all the last updated : same issue ! Giving up and going back to a working environment with a V13. Keep monitoring the subject, so if anyone has a solution...
|
7/25/2018 9:29 PM | |
Joined: 7/7/2010 Last visit: 11/13/2024 Posts: 15397 Rating: (2443)
|
Does anything on this forum link help at all? So your virtual PC is the windows provided virtual PC? How about adherence to the installation requirements? How about a suggested fix in this forum link which suggests how to force ALM to use local administrator account when it runs? If I were to guess, it is the virtualization technology more than anything else. Using VirtualPC is not supported according to the install requirements. However, the other suggestions may provide a work-around which is why I post the links. You can try it for yourself: (google.com) search box contents->[site:siemens.com win10 virtual pc or virtualpc tia portal v15 alm license manager]
|
science guy |
|
This contribution was helpful to1 thankful Users |
7/30/2018 1:25 PM | |
Joined: 7/22/2015 Last visit: 11/13/2024 Posts: 23 Rating: (5) |
Hi, Thanks for the comprehensive feedback. Problem solved by doing a fresh install and by installing ONLY Tia V15. I suspect Microwin to be troublesome. Thanks for the help ! Ronan
|
Follow us on