3/19/2024 12:05 PM | |
Joined: 3/11/2019 Last visit: 7/9/2024 Posts: 1511 Rating:
|
HI Kristof74, important for the PN/PN coupler is, the other side can be outside of the project -but- another controller on X2 including a valid configuraiton on this side is mandatory! Just removing the other PLC and leaving X2 open does not work. So question is: Is X2 configured in another systen including a PROFINET controller and is his side also connected? SIMATIC Bus links PN/PN coupler
regards sancruz |
Feedback appreciated, please rate |
|
Follow us on