7/25/2014 10:07 PM | |
Joined: 1/28/2009 Last visit: 10/11/2024 Posts: 6852 Rating: (1365)
|
Hello, There are some hints to be shared regarding your doubts in quoted STL codes:
For more help, please upload your project here.You are also recommended to read the following topics for more information:
I hope these comments help you! Hamid Hosseini |
Last edited by: hdhosseini at: 7/25/2014 10:11 PM |
|
This contribution was helpful to2 thankful Users |
7/26/2014 2:39 PM | |
Joined: 1/28/2009 Last visit: 10/11/2024 Posts: 6852 Rating: (1365)
|
Hello again, To answer all these question and the reason that programmer started with 124, multiply it by 2 and then add1 to the result, we need to access the source project.Perhaps a loop for iterative operation on a target area in a DB.As it explained in THIS picture,you need to pass the first 3 bits to make pointing address based on byte number.So 249 is transformed to 1992 (16#7C8).This is content of #pointer variable and CPU knows to read a byte from currently opened global DB that the byte number is 249.SLW in totat is a syntax to be performed.
I hope it helps, Hamid Hosseini |
This contribution was helpful to1 thankful Users |
7/27/2014 8:57 AM | |
Posts: 27 Rating: (0) |
Hello Mr.hdhosseini, I am very thankful to ur kind reply. now i catch some hints about this logic . |
This contribution was helpful to2 thankful Users |
Follow us on