2/9/2013 6:33 PM | |
Joined: 12/4/2009 Last visit: 5/3/2024 Posts: 452 Rating: (135) |
igor62il, use OB100 to set some user-defined bit, or useOB1_SCAN_1 information. More about OB1_SCAN_1 on thislink. Hope this helps, Regars. |
If this post actually helped, you may consider using the Rate button above. |
|
2/9/2013 6:37 PM | |
Joined: 1/28/2009 Last visit: 5/19/2024 Posts: 6839 Rating: (1359)
|
Hello , I have not worked on OMRON PLCs but I guess you want to find out how S7 CPUs executes after power on. Organization blocks are the interface of user's program to hardware.OB100 (OB101,OB102 with some differences which explained in STEP7 online manual) is available to determine your program reaction to CPU restart.In practice resetting some bits(or set some), making loops in manual,initialize communication and initializing production sequences are implemented. Best regards Hamid Hosseini Attachmentneu_start.zip (322 Downloads) |
Last edited by: hdhosseini at: 2/9/2013 6:44 PM |
|
This contribution was helpful to1 thankful Users |
2/9/2013 7:17 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Read suggested manuals too. Best regards, Hristo Mihalev
|
2/9/2013 8:01 PM | |
Joined: 5/27/2012 Last visit: 8/17/2023 Posts: 177 Rating: (0) |
To hdhosseini Yes,I want only one short puls only after power up on or reset PLC |
Follow us on