3/6/2014 10:34 PM | |
Joined: 5/29/2009 Last visit: 12/16/2024 Posts: 2 Rating: (0) |
I NEED ON SOME DIGITAL OUTPUT OF A MODULE 6ES7 132-7GD00-0AB0, IN SOFTWARE EVERYTHING IS CORRECT BUT THERE IS NO PHYSICAL SIGNAL MODULE, I CHECK THE CONFIGURATION OF HARDWARE AND THERE IS NO ERROR, ALL IS CORRECT, AND GENERATE A CFC WITH CHANNEL OUTPUT AND SIMULATING FROM SOFTWARE, NEW EVERYTHING IS CORRECT IN MY CHART SEE OUTPUT VARIABLES IN 1 BUT ALSO HAVE SIGNAL PHYSICALLY NOR ANY ERROR IS GENERATED. THERE ANY RESTRICTION FOR THIS MODULE OR ANY SPECIAL CONFIGURATION? HELPME PLEASE
AttachmentSCREENS_1.zip (237 Downloads) |
4/24/2016 3:19 PM | |
Posts: 5 Rating: (1) |
HI, digital output module is not normal DO unit . It's 6ES7 132-GD00-0AB0 that is installed on ET200iSP (profibus remote I/O).Base on manual and wiring diagram we have to only connect actuator(termian 1,2) and it is not necessary t o connect L+ and M for this module.I attached the photo of installed unit. Attachment4DO.zip (183 Downloads) |
Follow us on