11/24/2012 6:48 PM | |
Joined: 1/28/2009 Last visit: 7/11/2024 Posts: 6844 Rating:
|
Hello, Just to add some point while checking Diagnostic buffer. The sample I have working with would be like: [code] CALL "SCALE" IN :=PIW256 HI_LIM :=1.000000e+002 LO_LIM :=0.000000e+000 BIPOLAR:=FALSE RET_VAL:=MW100 OUT :=MD104[/code] Some possibilities are listed here: 1-If you select an Peripheral I/O address out of configured area, the CPU will go to stop if OB122(I/O access error OB) is not included in your CPU .Simply ensure that selected address is valid in HW.Config.For that right click on the I/O module and select "Monitor-Modify" to see what are the suggested addresses by STEP7 (pic#1 in attachment).Logs in buffer would be like this:
2- If you do not download FCs in the CPU.It is not rare in practice logs in Buffer:
3-And my final suggestion ,Please read the following manual especially chapter 6 for analog modules.Select your module and check the correct wiring.As an example see section 6.7.3 in which explains how an unused channel may lit SF LED. SIMATIC S7-300 S7-300 Automation System Module Data That is what I can share for now,Please provide us more information. Best regards Hamid Hosseini |
1/13/2017 9:06 AM | |
Posts: 1 Rating:
|
STOP caused by I/O access error (OB not loaded or not possible, or no FRB) FC number: 105 Module address: 46 Previous operating mode: RUN Requested operating mode: STOP (internal) AttachmentDiagnosticBuffer.txt (89 Downloads) |
Last edited by: Min_Moderator at: 1/13/2017 12:45:01 PMAttach Diagnostic Buffer |
|
6/12/2018 10:10 AM | |
Joined: 8/21/2014 Last visit: 7/15/2024 Posts: 995 Rating:
|
New question published by hdportal is split to a separate thread with the subject Problem in using "CPU clock memory" and "SCALE function" at the same time. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on