2/14/2011 6:24 AM | |
Posts: 17 Rating: (2) |
Hi dilip I think that you haven´t the bit 10 in the PZD1 (Control from PLC) in LOG1 (true). and for comunication between drive and PLC you can use direct perifery adress like PIW/PID ,PQW/PQD or which is better for data consistency in large aplication S7 block SFC14/SFC15. Look on the pictures: Attachmentimg.zip (738 Downloads) |
Last edited by: dfxdd at: 2/14/2011 8:09 AM |
|
2/14/2011 6:44 AM | |
Joined: 12/12/2005 Last visit: 3/17/2024 Posts: 180 Rating: (12) |
Hello dilip _123 I think you understand protocols, so here is one link and because you might need block in plc to help work with drive. http://support.automation.siemens.com/WW/view/en/22078757 If this link not open try search vwith this: MICROMASTER 4 & SINAMICS G Function block (FC14) to control an MM4 via Profibus-DP -Heksu- |
"Beer is proof that God loves us and wants us to be Happy"-Benjamin Franklin |
|
7/1/2014 11:46 AM | |
Joined: 9/1/2005 Last visit: 3/5/2024 Posts: 4097 Rating: (193) |
|
My Forum is the place to personalize your profile, |
|
Follow us on