11/13/2009 1:56 PM | |
Joined: 10/7/2005 Last visit: 9/13/2024 Posts: 3020 Rating: (1054)
|
Hello lean you didn't say which DI card you added to your ET200S. Please make sure it does exist in the module catalogue underneath your IM1516ES7 151-1AA04-0AB0 (i.e. if it doesn't then it can't be used with that IM151 and you most likely created the problem by dragging it in from a module catalogue of a different IM151). If the above is NOT the problem please try<CTRL>+<ALT>+<F11> in your HWconfig. I honestly can't tell you what this does, but this is the remedy according to the error code list which you can find here: Which meaning have the error codes (xxxx:yyyy) in STEP 7? I hope this helps and please let us know the outcome |
Cheers |
|
This contribution was helpful to1 thankful Users |
11/14/2009 10:55 AM | |
Joined: 10/7/2005 Last visit: 9/13/2024 Posts: 3020 Rating: (1054)
|
Hello again lean hmmm, this starts to sound like a case for Moulder & Scully, but since the "truth is out there" let's see if we can find it (all of this is from the X-Files for those of you who are not familiar with this slogan). To do so, I'd like you to post your S7 project to see if I (and/or others) can reproduce the problem. You can cut out all the "unimportant" stuff (e.g. integrated WinCC orflex andlogic Blocks) to keep the file size down if need be. Pleaselet us know too which Step 7 version you are using. As for your process image issue (and possibly your problem), I wonder if it is related to packing of addresses of the DI's (even though I am unableto reproduce it). By default every4 DI (or 4 DQ) ET200S module occupies addresses x.0 to 0.3 when dragged into the ET200S. Since thisleads to inefficient use of addresses ( x.4 to x.7of the same byte are "wasted") you can select a number of DI (or DQ cards) and use the "Pack Addresses" button to (well) pack the addresses (i.e. first 4 DI card then uses addresses x.0 to 0.3 and the next uses x.4 to x.7of the same byte). Since the Process image is set for a wholebyte address, you won't be allowed to change this for any "packed" card which uses bitaddresses x.4 to x.7 (it is now done on its partner card with x.0 to 0.3 addresses). |
Cheers |
|
Follow us on