Industry Online Support
Technical Forum
4/21/2009 8:09 AM | |
Posts: 487 Rating: (36) |
Hi Got funny problem when using VNC to goto a PC running a WinCC project The project is allways fullscreen with CTRL keys disabled , After logging in as an 'admin' user I can then ,using the 'send ctrl-alt-delete' function from vnc ,call the taskmanager and get access to the rest of the PC software . The problem is that suddenly the keyboard does not function properly anymore .For some reason the "Alt Gr" key seem to be pushed in . How do I unblock this key or get rid of it ? btw : were using win XP sp2 , dutch keyboard .and no,I cannot use another software ( vnc) to connect via remote unless somebody knows a solution to this second problem.SEE LINK This brings me to the original problem for going to this wincc PC using vnc .... This pc is a touchscreen PC 577B and if a user has to use the on screen keyboard to for instance change user level in wincc then the keyboard only works on the first use , the second time around the keyboard does not appear.This link did not solve the problem Because we are using SP2 , I presume that this supercedes hotfix 3 . Anybody with any ideas Greetings Eric |
Follow us on