11/12/2023 11:50 AM | |
Joined: 11/12/2023 Last visit: 1/10/2024 Posts: 3 Rating: (0) |
Hi folks, I have several problem with CU310-PN in STARTER I can see device with ip address 0.0.0.0 and some name (device was configured but returned to factory settings). If I try to change IP address with standard method I receive the error message something like "impossible to change" or like that. I try two computers with slightly different type of STARTER - same result. What can I check in this situation? ------------------------------------------------------------------------------------------ |
Last edited by: AutoGen_8145648 at: 11/12/2023 11:51:47Last edited by: Jen_Moderator at: 11/13/2023 11:24:24New subject after splitting |
|
Follow us on