12/10/2007 12:43 PM | |
Posts: 198 Rating: (17) |
dcomcnfg .. if everything (about network) is ok then you need to mess up with dcom settings .. reset them and try to reconfigure as manuals says.. |
12/10/2007 1:42 PM | |
Posts: 4 Rating: (0) |
I install the Simatic OPC Client - Scout on the interface node. But no changes.. Scout can'nt be connected to OPCServer.WinCC (see picture). |
12/11/2007 1:55 PM | |
Posts: 4 Rating: (0) |
I try SCOUT on 192.168.1.2 - is OK! But attempt SCOUT on the interface node - Error message . |
Follow us on