3/10/2006 3:11 PM | |
Joined: 8/31/2005 Last visit: 5/16/2024 Posts: 217 Rating: (40) |
Hi nkraven! Since the Firmware V2.4 contains only error corrections (see here: http://support.automation.siemens.com/WW/view/en/17504794) and no additional functionality, you can use the V2.3 from the hardware catalog to configure you CP 443-1. If you have no V2.3 in your hardware catalog, you should install the hardware updates from the internet (in the HW config editor via "Options -> Install HW Updates ...") |
Greetings, Chris |
|
3/13/2006 10:50 AM | |
Posts: 5822 Rating: (411) |
Hi nkraven, |
3/14/2006 8:31 AM | |
Posts: 15 Rating: (1) |
i updated the firmware version with the file that you recommended and it works now. Thank you for you support. Best Regards nkraven |
5/11/2018 6:42 AM | |
Joined: 6/19/2017 Last visit: 6/7/2024 Posts: 8150 Rating: (165) |
New question published by Siemens-man is split to a separate thread with the subject How can add the CP443-1 (6GK7 443-1EX30-0XE0) to the SIMATIC MANAGER?. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on