3/11/2009 9:07 AM | |
Posts: 2 Rating: (0) |
Hi, I am using DP DP coupler between two third party Profibus masters. In DP DP coupler is it neccessary to have the same no. of blocks in both the masters. i.e. While importing the GSD file in master 1 I selected a conversion rule of converting 32 bytes input to booland in Master 2 the conversion rule is to convert 16 bytes output to bool. This results in a scenario where in master 1 i configure 1 module of 32 bytes input in position 1 and in master 2 i configure 2 output modules of 16 bytes output in position 1 and 2. Is this a valid configuration. It is a urgent problem, can someone please help me out. Any input will be appreciable. Attached is the configuration that we have AttachmentDP DP network.pdf (315 Downloads) |
Follow us on