11/19/2009 9:44 AM | |
Posts: 103 Rating: (11) |
How are you all S5-compatible communication be used for data exchange with S7 stations, S5 stations and third-party devices. S7 communication can only be used for data exchange with S7 stations. You need one of the following SIMATIC NET PC software packages to be able to use these communication services including SIMATIC NET OPC server:
You need the following SIMATIC NET PC software to operate a PC station as PROFINET IO controller:
I don't know which case of the previous statement should I use? AttachmentNew Bitmap Image.zip (140 Downloads) |
11/19/2009 3:45 PM | |
Posts: 103 Rating: (11) |
thanks J_bell for your fast response now I don't have CP 1623 so I would not use it . I noticed that SOFTNET S7 Lean doesn't support profinet !! in the attachment picture I noticed that , SOFTNET S7 Lean support S7 COMMUNICATION & OPEN COMMUNICATION !!!! please describe this point to me ??? also in the table you will notice that , he doesn't assign any HW card to use with SOFTNET S7 Lean !! only he said << SIMATIC PC WITH INTEGRATED INTERFACE>> what does he mean by this statement?? thank for your attention. Attachmentall cards.zip (124 Downloads) |
11/20/2009 3:17 PM | |
Joined: 9/27/2006 Last visit: 4/18/2024 Posts: 12256 Rating: (2664) |
Hello ahmed; As far as yopur question 4) is concerned, you may find the information required in the following article: http://en.wikipedia.org/wiki/NDIS There are many ressources you can find elsewhere for such questions. Hope this helps. Daniel Chartier |
11/21/2009 8:55 AM | ||
Posts: 103 Rating: (11) |
|
|
Follow us on