2/22/2018 8:42 AM | |
Joined: 4/24/2006 Last visit: 9/29/2023 Posts: 8593 Rating:
|
Hello hsnaik, Perhaps the following links might help: Which connector cables are available for connecting to SIMATIC Panels? Here you can find the panels, that are released in combination with PC Adapter USB A2 Perhaps you can try to select MPI or Profibus: How can you transfer a WinCC flexible project via MPI/PROFIBUS to a Windows-based panel? Best regards Wizard |
This contribution was helpful to
1 thankful Users |
2/22/2018 9:03 AM | |
Joined: 9/21/2012 Last visit: 10/2/2023 Posts: 3778 Rating:
|
MP 177 DP is a Profibus panel, so select Profibus as the connection when you use the PC ADAPTER USB A2. |
Follow us on