Industry Online Support
Technical Forum
4/16/2014 10:21 PM | |
Posts: 1 Rating: (0) |
I have an S7 program attachedhere for an RFID scanner that I am unable to get to work correctly. The hardware involved is an RF630R which is connected to the profibus network with a RF160C communication module. My "Ready for Next Command" bit in FC20 is not active. Also, on the RF160C itself, the red error light blinks once, which is the signal for module is ok but needs a restart. I'm not sure if that is being done.. Any suggestions? Thanks! AttachmentC:\Users\supebx\Desktop\Rfid.zip (340 Downloads) |
4/17/2014 1:53 PM | |
Joined: 10/1/2013 Last visit: 5/8/2024 Posts: 605 Rating: (71) |
Hi, which error LEDs blink? Sad I have no time to look at your projekt, but you could give us more information. |
Follow us on