2/8/2011 9:33 AM | |
Joined: 12/12/2005 Last visit: 3/17/2024 Posts: 180 Rating:
|
Hi, I think I have all basic programs to work with S5,S7 and panels, but time to time coming this kind of problems frequency converter, servos,etc. ... SO, I wonder if there is (Siemens)list where you can seedevice and programming program needed, free download or order?. I just found Masterdrive Mc that DriveMonitor(free) is not enough, i´ll need to order Drive Es Basic. It takes too much time to find out from forum, this kind of information. So I hope, please! tell me where is information or list, to help find outif we need or not? What program? I think there is not...(www.google.com). Best regards -Heksu- |
"Beer is proof that God loves us and wants us to be Happy"-Benjamin Franklin |
|
2/9/2011 1:20 PM | |
Joined: 12/12/2005 Last visit: 3/17/2024 Posts: 180 Rating:
|
Hi Hristo, Almost all cases DriveMonitor is enough? read this first: /tf/WW/en/Posts/41078#top Thanks for your opinion [schnippschnapp] new question is splitted to I need to upload Masterdrive parameters and see diagnostic and faults and alarms. Regards -Heksu- |
Last edited by: O_Moderator at: 2/9/2011 1:52 PM"Beer is proof that God loves us and wants us to be Happy"-Benjamin Franklin |
|
2/9/2011 1:57 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating:
|
Hello, It is useful if all the drives are imported into Step7 project and then instead of using serial cable use profibus or ethernet cable to connect to the drives. What is Drive ES? - Drive ES Basic V5.4 SP5 If you have DriveMonitor (alone) and serial cable you could do everything with the drives. To buy this packge only to be possible to open the drives via Simatic Manager and there to update the project. To open to see faults and alarms history...leave it for the moment away. Best regards, Hristo Mihalev |
Last edited by: UMENCHO at: 2/9/2011 2:08 PMLast edited by: UMENCHO at: 2/9/2011 2:04 PM |
|
Follow us on