4/28/2016 12:15 PM | |
Joined: 2/23/2016 Last visit: 2/14/2024 Posts: 36 Rating: (2) |
Hi i upgrade my project with cpu 416 3DP from pcs7 v 6.1 to pcs7 v8.0.all functions working correctly and all transmitter and positioner detected in PROFIBUS PA segments except a few positioner and some transmitter.but all instruments working correctly with pcs7 v 6.1 but dont work in pcs7 v8.0. please help me for this problem. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 4/28/2016 1:21:28 PMNew subject after splitting |
|
4/28/2016 2:00 PM | |
Joined: 3/14/2008 Last visit: 5/14/2024 Posts: 2066 Rating: (928) |
Have you gone from v6.1 to v8.0 instantly? Or did you follow the correct path-> v6.1-v7.0-v7.1-v8.0? |
If I could help you, you can use the RATE button. Thank you. |
|
5/3/2016 7:46 AM | |
Joined: 3/14/2008 Last visit: 5/14/2024 Posts: 2066 Rating: (928)
|
Hi Moji, The correct path is to upgrade from version to version. Attached is the migration strategy if you want to go to PCS7 8.1. You will need first the following manual: Software update without using new functions from v6.x to v7.1 Then you can use the following manual: Software update without using new functions to v8.1 Are you planning to re-engineer the process by using APL library? Then you will need different manuals-> Software update with new functions. In short, you will have to upgrade your blocks to v7.1 sp4 in order to use them in PCS7 8.1. |
Last edited by: Oreca at: 5/3/2016 8:38:54 AMForgot attachment If I could help you, you can use the RATE button. Thank you. |
|
5/17/2016 11:29 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4772 Rating: (123) |
New question published by Msc.Automation Eng. is split to a separate thread with the subject PCS7, upgrade project from V6.0 to V8.1. Best regards |
Follow us on