12/27/2006 11:10 AM | |
Joined: 4/24/2006 Last visit: 7/12/2024 Posts: 8711 Rating: (1166) |
Hello Vkart, Have you seen the following manual: http://support.automation.siemens.com/WW/view/en/12429336 chapter 5.7 Look also at the right to the 'info' here you can download some example's. Hope this will help. Best regards, Wizard |
12/31/2006 7:55 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (318)
|
Hi Vkart, For the ET 200S is a Puls Width Modulation module available, maybe is that something for you. See the FAQ Decentralized output of variables with the 2PULSE module on ET200S and the handbook Technological Functions ET 200S When you want to do it on your own, then consider that this is not so accurate as a hardware module. If you use a time-OB (OB35) then you can switch every 5mS when the OB35 is placed on that time (the rest of the program will be getting trouble when you want to do other things also fast. Then you have to make in steps of 5mS some programming that is making what you want. Also with the CPU 314C is some possible, see the handbook S7-300 Automation System CPU 31xC Technological Functions please see also under info on the right where some examples are placed of the technologic features of the CPU 31xC. |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
3/27/2017 10:33 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4770 Rating: (123) |
Best regards |
Follow us on