Industry Online Support
Technical Forum
10/24/2006 1:47 PM | |
Joined: 10/10/2005 Last visit: 7/18/2024 Posts: 1917 Rating:
|
Hello, regarding to your inquiry in refer to the performance there are the following reasons: Check your hard disk and the virtual work memory and when it is possible you should increase these memories. Consider the informations of the readme file by 3.2 Memory Requirements. Is there a virus scanner which is active during you work with STEP 7? We recommend to deactivate the virus scanner if you work with STEP 7. We recommend also to save your projects with the function "Save as..." together with the option "With Reorganisation (slowly)". Please see also our FAQ in this regards: "Notes on Optimizing Performance", which do you will find by the entry id: 20440472. Check also the requirements in refer to the installed SIMATIC software, whether your PC is suitable for these versions. Home page of the customer support: http://www.siemens.com/automation/csi_en/product With best regards Cicero |
Follow us on