6/6/2019 12:25 PM | |
Joined: 9/27/2006 Last visit: 2/20/2025 Posts: 12339 Rating:
|
Hello hrthrt; The following documents describe how to configure the Modbus TCP functions on S7-1500 CPUs: https://support.industry.siemens.com/cs/us/en/view/102020340 https://support.industry.siemens.com/cs/us/en/view/100633819 Hope this helps, |
6/6/2019 3:23 PM | |
Joined: 5/6/2010 Last visit: 2/7/2025 Posts: 2012 Rating:
|
Hello hrthrt, maybe is this document helpful Modbus Communication with MB_Client and MB_Server The connection parameters can you set at the DB - please look at the attachment. The IP-address 0.0.0.0 means that a request can come from every IP.. Hope this is also helpful. regards AttachmentMB_server.pdf (141 Downloads) |
Last edited by: Jen_Moderator at: 06/07/2019 08:26:26Optimized link. |
|
This contribution was helpful to
1 thankful Users |
6/7/2019 9:03 AM | |
Posts: 8 Rating:
|
So i just create db and configure parameters in it ? I though I should do it in block which auto creates with adding FB in program . |
Follow us on