2/15/2023 11:50 AM | |
Joined: 5/30/2022 Last visit: 8/13/2024 Posts: 563 Rating: (94) |
Hi AutoGen_5043068, You should always select a system according to the needs of your project, I attach some information that will help you when choosing a system. SIMATIC S7-1500 S7-1500R/H redundant system If you have any questions, please let me know so that I can help you.
|
If this information really helps, you could use the Rate function. |
|
2/16/2023 5:40 AM | |
Joined: 10/3/2022 Last visit: 2/16/2023 Posts: 2 Rating: (0) |
Hi Hazard_7, Thank you the response. However, I am looking for more of a general unique differentiator between the both controllers. For example, I know that the S7-400 allows the user to Configure in Run, that gives the S7-400 a huge advantage over the S7-1500. Additionally, I believe the S7-1500 has faster processing power. Would you be able to share more information on these key differentiators? |
Follow us on