3/7/2018 11:37 AM | |
Joined: 4/8/2016 Last visit: 10/24/2024 Posts: 133 Rating: (45) |
Hello, first a question: Why do you want to exchange the CPU? If you just want more PO you do not have to exchange the CPU 410-5H. You can upgrade them online (from PCS 7 V8.1) with an Expansion Pack. Have a look at the following document (Chapter 2.6.): https://support.industry.siemens.com/cs/ww/en/view/96839331 If you still have to exchange the CPU I would do the following:
|
Kind regards |
|
3/8/2018 10:33 AM | |
Joined: 4/8/2016 Last visit: 10/24/2024 Posts: 133 Rating: (45) |
The newer firmware version V8.2 of the CPU is compatible with the older firmware versions, so you do not have worry about this. 1. Readback Parameters: See Chapter 16 in the following manual: https://support.industry.siemens.com/cs/ww/en/view/109755021 2. Book back PO: Right click on the Charts folder and use "Charts > Book Back Process Objects". 3. Nothing special that I'm aware of. |
Last edited by: 51N3P at: 3/9/2018 1:36:55 PMKind regards |
|
3/8/2018 11:24 PM | |
Posts: 5 Rating: (0) |
Hi, Thanks so much for answers, will do the job by next Wednesday and will update everyone here. |
3/9/2018 3:05 AM | |
Posts: 5 Rating: (0) |
Do you know how could I download the English Version of that document? |
3/9/2018 6:35 AM | |
Posts: 5 Rating: (0) |
Thanks Daniel |
Follow us on