7/14/2019 5:23 PM | |
Joined: 9/27/2006 Last visit: 2/18/2025 Posts: 12337 Rating:
|
Hello Pavel; I'm afraid such a command or instruction does not exist in Step 7, classic or TIA Portal: What is the significance of the initial and actual values of a data block? https://support.industry.siemens.com/cs/ww/en/view/837001 Since the initial value does not continue to use the initial values, there is no need to perform the opposite procedure, i.e. to load the values from the "Actual value" column to the "Initial value" column. There is no menu command for this either in STEP 7. The following instructions are used in some uncommon configurations for saving the actual values of a data block as initial values. This procedure can either be conducted directly within an STL source or by saving the values with Excel. Hope this helps, Daniel Chartier |
8/1/2019 8:53 PM | |
Joined: 4/23/2015 Last visit: 6/12/2023 Posts: 168 Rating:
|
Dear huggy_d1, thank you. It looks pretty complicated. I think I have to use the method proposed above by Kai.A. |
Follow us on